(0)| 8/21/2013 2:26 PM | |
|
Posts: 3093 Rating:
|
Hello Damayanti, Modbus libraries are available for the integrated PN interface of IM151-8 as general version and one especially to connect numerous PAC3200. These libraries can be used with TIA V11 as well - with one limitation: the wizard can only be used with STEP7 5.5. You can find detailled information and a demo version at www.siemens.com/s7modbus. Regards, Kaulquappe and this is the link to migrate the Modbus block from STEP7 V5.5 to TIA V11/V12 |
Last edited by: Kaulquappe at: 8/21/2013 2:30 PM |
|
Follow us on