(0)| 10/29/2013 4:10 PM | |
|
Posts: 13 Rating:
|
Hello Experts, Can anyone help to fix a System Alarm warning I get when compiling a project using WinCC Flexible 2008 Advanced Sp2? The warning at compile shows: "Warning: Internal warning (detail: system message 80015: missing text - object type: SYSTEM_MESSAGE).". When I right click the warning and I click on "Go to Usage", nothing shows up. I went to the "System Events" in Alarm management in the Project tree and there was no text against the 80015 alarm number. I added the text "DOS or database errors" against the alarm number 80015. However, still the compile shows the same message as above. Now if I right click on the warning, the "Go to usage" is grayed out and is not available. A screenshot of the System Alarm text is atached. Is it because the text is not corrct or something wrong with the database I am using. Note that I can download to the file to HMI and the program runs without warning in runtime. Can anyone help? Thanks in advance. Attachment80015_WinnCCFlex2008Sp2_alarmIssue.pdf (314 Downloads) |
Last edited by: O_Moderator at: 10/31/2013 9:57 AMnew subject after splitting from /tf/WW/en/Posts/96057#top |
|
This contribution was helpful to
|
|
Follow us on