(0)| 11/9/2013 4:26 PM | |
|
Joined: 3/14/2008 Last visit: 1/15/2026 Posts: 2233 Rating:
|
Hello, I'm using v8.0 sp1 with advanced ES. I created a Control Module Type named Motor_Type. In there is a feedback input, control output and offcourse a MotL block. I would like the MotL block name to be the same as the Control Module name, or at least specify this at Advanced ES. AdvancedES can only write in high level CM, so I have to make a assignment in the high level CM to forward the Control Module name to the MotL block. However, when I do this, strange things happen: a copy is added to the Control Module and my chart names are named the same as the Control Module Type with [] abbreviations. I tried to do this with the Comment field and this works.... Is there a way to accomplish this? I can edit the block names in AdvancedES manually, but this is time consuming... Thxx!!! |
Last edited by: Oreca at: 11/9/2013 4:59 PMLast edited by: Oreca at: 11/9/2013 4:27 PMIf I could help you, you can use the RATE button. Thank you. |
|
Follow us on