(0)| 2/2/2012 6:43 AM | |
|
Joined: 8/31/2010 Last visit: 12/6/2025 Posts: 1525 Rating:
|
Hello Martins_Eng, I don't know if i got your question right. Check this - How through external switching can you use a 0-10V analog input on a makeshift basis also for 0-20mA?(Ideally this should be applicable to S7-1200 also) To address the analog input go and check the AI address from the Inspetor Window (in the bottom of TIA Portal) -> under that select Properties area -> Select AI2 in your S7-1200 CPU -> under that select I/O Addresses -> Check the start address specified there. If the Start Address is 64 (default), and the number of channels of that module is two; then you can access it as %IW64:P and %IW66:P |
|
Like it? Rate it! |
|
This contribution was helpful to
|
|
| 11/16/2013 7:54 PM | |
|
Posts: 3 Rating:
|
Thanks for this post it is very helpfull |
This contribution was helpful to
|
|
Follow us on