(0)| 1/2/2008 2:08 PM | |
|
Joined: 4/18/2006 Last visit: 1/9/2026 Posts: 20 Rating:
|
Hi MS_LAZZ on internet you find the answer. Here an extract: ---------------------------------------------------------------------------------- Measuring systems with EnDat 2.2 and EnDat 2.1 - compatibility(ID: 22731584) The EnDat interface is the bidirectional interface for measuring systems from Heidenhain. EnDat 2.1 is the standard in recent years and allows absolute position values to be transferred. In addition to the digital position values, analog incremental signals are transferred with 1Vpp. These are interpolated in the drive converter for fine resolution. More detailed information can be taken from the attached excerpt from the following document "Rotary encoders, Status 11/2005" from the Heidenhain company. ------------------------------------
Software involved: AttachmentEnDat2_1-2_2_76.pdf (510 Downloads) |
Follow us on