(0)| 11/23/2013 2:20 PM | |
|
Posts: 2 Rating:
|
Hi I'm a student of KHLim in Belgium. I am doing a thesis on Variotherm Injection moulding. I have a Siemens S7-1200 PLC here which needs expanding. It regards a S7-1212C CPU and a PM 1207 PSU. All the In and Outputs on this CPU are taken, which requires me to get extra modules for my in and outputs. I need atleast 2 AI, 1 AO, 2 DI and 2 DO. What cards can I use? The problem is that I don't have any room for expansion in my current cabinet. Can I put extra modules in an other cabinet (which will be the cabinet for all the Variotherm control) and communicate with the CPU? Since I wanted a fast answer I'm gonna try to put it here on the forum before emailing Siemens, since it is weekend Can anyone of you help? Thx in advance Siemen Gorissen
AttachmentCabinet.pdf (310 Downloads) |
| 11/24/2013 11:49 AM | |
|
Posts: 2 Rating:
|
Thank you very much for the reply Do I need an extra PSU to power these expansions, since it requires 24V DC? Thx
|
Follow us on