(0)| 1/25/2014 8:27 PM | |
|
Posts: 16 Rating:
|
Dear Sir I am installing CNC contoller 802Dsl G/N-plus on a STRIPPIT punch machine (the former controller(CNC) was G.E.) I attached the specification of controller. this machine is equipped with Loader/Unloader , so for automatic operation of Loader/Unloader in middle operation of CNC program ,I must move axes in PLC program. I dont need permanent PLC axis , only by variables VD570X0000 ,VD570X0004 AND V26000001.1 ,V26000001.2 how I can travers axes in AUTOMOD ? please send me the PLC program Subroutine for control axes in this situation. For punch mode operation , I must use high speed I/O of MCPA board. the Parameter are sets as : MD10350 :2 MD10360 :2 MD10366 :10101 MD10368 :10101 when I active inputs 9-16 on MCPA , the VB29001000 is active , and I observe situation in the PLC.in PLC program for high speed 9-16 on MCPA board, when I active VB 29001004 ,The PLC go to STOP mode. I checked the high speed 9-16 on MCPA board with VB28001008-VB28001011 ,but I dont have any output on terminals of MCPA board. how I sets Machine Data , I have outputs on MCPA? CONTROLLER CNC-802 Dsl G/N plus specifications : Module : SZVD7YL0001133- 6FC5370-0AA00-2BA1 Hardware- version : 03.02.00.01 Hardware Revision : E
Software : 802Dsl G/N plus Version : 01.04.07.05 Internal Version : 01.40.70.00 Bios-Version : V02.01.00.00
HMI-Version : 05.06.57.03
Base System : 67.12.04 : 19/06/12 Numeric ConSI 67.11.00E : 67.12.06 06/12/12 Ncks 802d-ng2 : 67.12.06 06/12/12
PLC System : E 04.05.12 03/04/12 PLC application : (file name)
Subroutine Library 802Dsl V02.00.15 AttachmentCONTROLLER CNC-Specification.pdf (101 Downloads) |
Follow us on