1/28/2014 8:57 AM | |
Posts: 215 Rating: (6) |
Hello Fatso, to make sure we are talking about the same: do you refer the following website? https://www.automation.siemens.com/mcms/programmable-logic-controller/en/logic-module-logo/application-examples/Pages/Default.aspx?HTTPS=REDIR, 10th zip file? I have got a 6ES7 315-2EH14-0AB0 with PN/IE interface onboard and it works also fine. As far as I know there is no difference in communication of differrent S7-300 types if they are equipped with an Ethernet port. Did you make a ping check? Did you check all addresses to be in the same range =.=.=.# ? Regards |
Follow us on