12/5/2008 7:57 AM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Hello Yes, there hasconstraints where you can put IM308C in the rack. See in manual (page 120). In this manual you also can find further information about how to build Profibus system with IM308C. 1.IM 308C - MLFB: 6ES5308-3UC21 2. MEMORY CARD - See in manual page 322 3. Profibus connector - See in the same manual page 74 4. Software archive: COM ET100 V2.1 (this will be harder to find ) 5.6ES5894-0MA04-0UG4 STEP 5 BASIS V7.2, CD, UD, (G/E/F/I/S) 6.6AG1153-1AA03-2XB0 SIPLUS ET200M IM153-1 reagrds |
2/17/2009 3:04 PM | |
Posts: 8 Rating:
|
You will also need a programmer(PG or external)for the memory card to export comprofibus file to the memory card. Butthatis maybe obvious |
3/5/2014 12:55 PM | |
Posts: 340 Rating:
|
new question is splittet to IM318, change to S7 I/O Module, (153-1 and IM153-2). |
Follow us on