(0)| 4/1/2014 8:19 PM | |
|
Joined: 12/13/2012 Last visit: 3/18/2025 Posts: 7 Rating:
|
I have a strange problem with my s7-1200 project when I want to use the webserver. It seems that my project doesn't link "Name" and "Addresses" in my PLC tags when used in my webserver. By example following is in the PLC tags table:
When I change test in the webserver, Variable Status page, MW250 won't change. If I change MW250, test won't change. This gives a problem when I want to use user defined pages with: <!-- AWP_In_Variable Name='"test"' -->
Has anyone an idea what the problem is? Attachmentwebserver.zip (180 Downloads) |
Last edited by: CS Moderator at: 4/2/2014 1:58 PMPicture part of the attachment |
|
| 4/3/2014 10:16 AM | |
|
Posts: 3 Rating:
|
try [code]<input type='text' name='"test"' value=''>[/code]
|
Follow us on