(3)| 5/29/2014 9:08 PM | |
|
Posts: 51 Rating:
|
ok thanks mr.hosseini i will check n get back you soon with testing... weather is it possilbe for TIA V12 with Wincc Professional?????? what to do??? for that??
|
| 5/29/2014 9:40 PM | |
|
Posts: 102 Rating:
|
hello, The simplest and best way to do this is to let SIMATIC manager do it for you. In the hardware manager select the plc and then go to Options -> Report System Error. Fill out the info in the dialog window. The really important tabs are the OB Configuration tab and the CPU Stop tab. Beyond that the defaults handle the rest. Hit the generate button and all of the hardware diagnostics code is automatically generated and done. You can add your own processing code in each section to perform system shut downs or trigger other actions within the pre-configured blocks if you want.
Now in Siemens HMI all you have to do it subscribe to the messages which involves a few check boxes in the alarm setup and alarm window properties. Check out this faq:http://support.automation.siemens.com/WW/view/en/22319131 There is also a PDiag add-on for Step 7 that provides this same message functionality for all of the process alarms in a system. So all of the alarms are configured and managed in the PLC and the HMI becomes just a window to them. It works great and best of all with the Profinet CPUs you can open up the CPU web page and view all of the system alarms and hardware errors without any special software just by looking at the CPU messages. |
This contribution was helpful to
|
|
| 5/30/2014 8:37 AM | |
|
Posts: 51 Rating:
|
thanks all i will checked and get back to you soon.... |
| 5/30/2014 5:20 PM | |
|
Posts: 559 Rating:
|
For The configuration of the System Error the below link will be help ful to you. How can you report S7 system errors in WinCC? and How can you have system error messages from a SIMATIC S7-300 / 400 displayed in WinCC flexible? |
| 5/30/2014 8:13 PM | |
|
Posts: 51 Rating:
|
Hi PG.. I didnt find any system alarm configuration In TIA....Could you expalin???
|
Follow us on