(0)| 5/27/2014 11:26 AM | |
|
Joined: 6/1/2010 Last visit: 2/17/2025 Posts: 36 Rating:
|
Hello In plc data type the way to search every variable use is not clear. In the attachment finding the use of for exemple “temperature” in the data type “type_motor” do not work with cross reference the only way is to delete it in the type declaration, compile and see where the error occurs. Not the best method but it’s the only one I find. If anyone as another it can be helpful. Have a good day Attachmentrecherche_dans_projet.zip (227 Downloads) |
Follow us on