(1)| 5/30/2014 7:42 PM | |
|
Posts: 25 Rating:
|
Hi, I'm new to the Tia Portal software. I'm trying to setup a system that uses isochronous IO in the PLCSIM simulator. I created a S7-1500 device and a ET200S device for remote IO and connected them together with a Profinet cable. In the S7-1500 program I added an OB61 block that does something simple for now. The compiler gives the following error: No IO system is assigned to OB Synchronous Cycle. How can I do this assignment? When hovering with the mouse over the profinet connection in the Devices and Network view, a popup shows the text: Sync-Domain_1. So I think I should link the OB61 cycles to this sync domain. But how?? Is there a good document about this? I found this document (S7Takts_e.pdf) describing the settings for Isochrone mode. But I think it is related to older software, because in TIA Portal the settings seem to be completely different. Is there a TIA Portal document version of this document? |
Last edited by: make_it_move at: 5/31/2014 11:05 AMLast edited by: make_it_move at: 5/31/2014 9:19 AM |
|
| 6/5/2014 5:03 PM | |
|
Posts: 25 Rating:
|
Also when I select the network connection. I get the following information. See picture. Is there some indication of the problem in this information? |
Follow us on