(0)| 6/6/2014 11:12 AM | |
|
Joined: 4/8/2010 Last visit: 7/3/2025 Posts: 96 Rating:
|
Good morning I must manage a rotating BLADE (200Hz motor) into automating cell. Actually a manage a deceleration ramp from two cutting and it's not OK They have suggested to me to put parameter 844 = 0 and put OFF1,2,3 = 0 for free rotating blade when I don't cut (From two cutting operation motor will running free). Before start a new cut with parameter 1200 = 4 (Starting Fly) Simodrive search a actually motor rpm and restart faster. (There are a parameter to read for have a information about acceleration ramp finish ?) For stop motor faster in case of Emergency STOP use parameter 1231 = 5 (Brake motor with CC current) and set only OFF2 = 1 ? In attached file we have a configuration with standard use : Only with deceleration ramp Thank-you for your HELP AttachmentMandri_12_8285_Profinet.zip (186 Downloads) |
Follow us on