(0)| 6/30/2014 7:01 AM | |
|
Posts: 4620 Rating:
|
Hello germynator, you have marked the CPU connection 314IFM as Profibus DP? are you sure? This CPU (IFM)as faras i know does not have the Profibus DP port onboard you have ONLY MPI Port, on the PC side which adapter you have? also have a look: SIMATIC HMI WinCC flexible 2008 WinCC flexible 2008 Runtime |
Last edited by: Ste39 at: 6/30/2014 7:07 AM |
|
| 7/3/2014 4:59 PM | |
|
Posts: 4620 Rating:
|
Hello germynator, recapping you want to connect an HMI (PC) with the S7 314 IFM, you've really only a RS 232? you want to communicate via Modbus for strength? if you have a communications processor says the FAQ below: How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI? |
Follow us on