(0)| 10/11/2013 2:55 PM | |
|
Posts: 206 Rating:
|
Hello Subin, the Siwarex WP231 is a weighing module only for weighing. It has no dosing functionality. Only the zeroing a the beginning of the dosing can be made with the Siwarex WP231. The dosing function that you described you have to realize in the PLC. If you need a module with dosing functions like you described you would need the Siwarex FTA. The Siwarex FTA is a S7-300/ET200M module and can't be used wilt S7-1200. The manual and a quick guidefor the Siwarex WP231 you find here: http://support.automation.siemens.com/WW/view/en/64722267/133300 If you look at the example program you find the structure of the DB withcommentsin it: http://support.automation.siemens.com/WW/view/en/66825585 Regards ABenno |
| 2/17/2014 6:01 AM | |
|
Posts: 84 Rating:
|
Sir, I have gone through the Sample project on SIWAREX WP231on the Entry ID:82454336. http://support.automation.siemens.com/WW/view/en/82454336 But i didn't understand the consept of filling. In the project it using a 3kg load cell and and weighing wall dowels. Let say one carton consist of 1000 wall dowels and got a total weight of 500g. so each wall dowels weight 0.5g. so the target weight is 500g. please explain me how it control the output when reaching 500g. I just confuse as in the SIWATOOL configuration file its difault limit values Limit1=99% and limit2=50% if so as the max weight set is 3000g. for the slider to close,from what i understand it should close when weight value reach 2970g. So how to control the product to target 500g. Also didnt understandy why it used CSM 1277 ethernet switch and link with siwarex. Is it just to configure siwarex with siwatool or need to communicate online? I already done the project for liquid filling with SIWAREX WP231 for filling 3kg and 5kg. As got different kind of liquid the density also vary. So i need to set different limit values for different products to cut off the valve at the set limit values. As i cannot use siwatool all the time to change the limit % to change a product and also the DR6 is also locked. i used the modbus communication in parallel to the plc so change the limit values. Now the fillier is set to production.. The one issue is sometime the read write command not working even the modbus is communicating properly. the other issue is i use the set zero command which is direct command through plc. but it also sometime fail.. I am waithing for the new firmware which suppose to unlock all the data records and can control all settings through the plc. Anyhow this sample project give me a hope. but confused as because of the weighing procedure.. will this sample project can be useful for my liquid and powder filling for a machine with multiple weight filling.. |
| 3/17/2014 4:44 PM | |
|
Joined: 9/1/2005 Last visit: 1/9/2026 Posts: 4114 Rating:
|
follow up question published by lilluis split to a seperate thread with the subjectpower supply when connecting the WP231 with the PLC. Best regards CS Moderator |
|
My Forum is the place to personalize your profile, |
|
| 7/14/2014 3:42 PM | |
|
Posts: 176 Rating:
|
New question split intowp231 v11 s7 1200 communication program. With best regards, Narrator1
|
Follow us on