(0)| 9/11/2007 11:26 AM | |
|
Posts: 5822 Rating:
|
Hello, due to the Interface you intend to use, the PROFIBUS Interface of the CPU, you are restricted to a view possibilities. These are:
The DP Protocol would than be used that way that the PC is DP Master and the CPU is DP Slave, the way to configure the CPU as DP Slave is explained in the Configuration Manual in STEP7. |
| 7/15/2014 11:39 PM | |
|
Posts: 176 Rating:
|
New question split intoDP- DP coupler to exchage process data with ABB dcs on profibus protocol. With best regards, Narrator1
|
Follow us on