(1)| 7/10/2014 5:43 PM | |
|
Posts: 378 Rating:
|
Dear mjrv,
Yes you can back up by RS232/PPI cable. Create a new blank project wincc flexixible with your device type >> Project >> Transfer >> Backup , then follow the instructions. Note that you can only make backup if only the project was previously downloaded with back transfer option enabled. To restore: OP77, and OP277 are two different devices thus you need to reprogram/modify it to suit OP77 functions.
I am confused here, this OP277 is new? Without program? If no program, you can't see any user interface screens plus function keys are nothing without the program. Regards |
| 7/28/2014 9:52 AM | |
|
Posts: 4620 Rating:
|
Hello mjrv, What WinccFlexible you have exactly? 2008 ---> SP? Update for WinCC flexible 2008 Service Pack 3 |
Last edited by: Ste39 at: 7/28/2014 9:58 AMUpdate SP3 |
|
Follow us on