8/12/2014 8:54 AM | |
Joined: 11/16/2012 Last visit: 8/13/2025 Posts: 228 Rating:
|
Hi Kashir, for studying the basic of PCS 7, I recommend to you the 'Getting Started' manuals. You will find them in the following thread: All Getting Started manuals for PCS 7, BATCH and Route Control Also the following page is very helpfulfor the work with PCS 7. Here you will finda lot of information and solutions: www.siemens.com/industry/onlinesupport/pcs7 Regards jumo |
This contribution was helpful to
1 thankful Users |
8/12/2014 9:41 AM | |
Posts: 19 Rating:
|
Besides the manuals, I also found this. It does not explain all possibilities, but you can get an idea of the steps that you should follow to create compile and download, and also what you should expect while creating your hierarchy. I hope you find it useful ;) Kitchen_Project |
Last edited by: O_Moderator at: 8/12/2014 9:56 AMlink corrected Last edited by: Drugüi at: 8/12/2014 9:43 AMLast edited by: Drugüi at: 8/12/2014 9:42 AMLast edited by: Drugüi at: 8/12/2014 9:41 AM |
|
This contribution was helpful to
1 thankful Users |
8/12/2014 1:45 PM | |
Joined: 11/29/2011 Last visit: 2/4/2025 Posts: 1362 Rating:
|
Hi, Wincc is the integrated OS part of PCS7. There are different configurations: -OS Single Stations ( this station run the Server application and provide user interface for operators), -OS servers (only run the Server apllication), -OS Clients (provide user interface for operators). The ES (Engineering station) is only for managing engineering work on the code. The AS is the PLC basically. There are many other bricks in PCS7 but do not worry about them in the first run. I think you need to cliarify what your client wants. Have a look at this manual, Chapter 2: http://support.automation.siemens.com/WW/view/en/68157327 This should give you a very good overall understanding of the system. If you can identify the archtecture, it is easy to find out what the client ask for. Make sure you always double check with the client. Also a big help to read trough the PCS7 getting started manuals, they provide a lot of infomration about the system architecture. Your local Siemens representative can also help you with selection. Cheers: |
- What you read here, please check with manuals and your requirements. |
|
This contribution was helpful to
1 thankful Users |
Follow us on