12/20/2011 12:12 PM | |
Posts: 1776 Rating: (95)
|
Hi, here is the link. Have attention, that there are available 6 Updates for V7.0 SP2 https://support.automation.siemens.com/WW/llisapi.dll?aktprim=100&lang=en&referer=%2fWW%2f&func=cslib.csSearch&siteid=csius&extranet=standard&viewreg=WW&groupid=4000002&objaction=cssearch&content=adsearch%2Fadsearch%2Easpx |
12/20/2011 3:48 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Because above link is not working (at least for me). http://support.automation.siemens.com/WW/view/en/44452271 You need to have a valid WInCC 7.0 installation plus license for it in order to update to SP2.
Then use http://support.automation.siemens.com/WW/view/en/56640906 And on January 2012 wait for SP3 of WinCC 7.0 supports 64 bits platform... Upps!SP3 http://support.automation.siemens.com/WW/view/en/55987264 came a little bit earlier. Best regards, Hristo MIhalev |
Last edited by: UMENCHO at: 12/22/2011 9:30 AM |
|
9/23/2014 9:44 AM | |
Joined: 9/17/2014 Last visit: 2/17/2022 Posts: 9 Rating: (1) |
Hello, This is link +https://support.automation.siemens.com/WW/llisapi.dll/csfetch/44452271/WinCC_V70SP2_download.zip +https://support.automation.siemens.com/WW/llisapi.dll/csfetch/44452271/WinCC_V70SP2_download.z01 +https://support.automation.siemens.com/WW/llisapi.dll/csfetch/44452271/WinCC_V70SP2_download.z02 +https://support.automation.siemens.com/WW/llisapi.dll/csfetch/44452271/WinCC_V70SP2_download.z03 +https://support.automation.siemens.com/WW/llisapi.dll/csfetch/44452271/WinCC_V70SP2_download.z04 +https://support.automation.siemens.com/WW/llisapi.dll/csfetch/44452271/WinCC_V70SP2_download.z05 g |
This contribution was helpful to2 thankful Users |
Follow us on