(0)| 10/22/2007 12:02 PM | |
|
Posts: 23 Rating:
|
HELLO MR DANIEL CHARTIER........ |
| 10/27/2007 12:21 PM | |
|
Joined: 9/27/2006 Last visit: 1/16/2026 Posts: 12481 Rating:
|
Hello diar; Sorry, but have you followed J-Bell's earlier sugfgestion: "have you read the chapter 6 in this Manual? CP 341 Point-to-Point Communication Installation and Parameter Assignment If not you will find in the FB 7 and FB 8 the parameters" You will find there basic explanations for allrequired parameters for the FBs supplied with the CP341. Notice also that you do not need to open the block parameters for them to function. You simply cpopy or drag them from the Library into the network (Lad or STL view) that you need to program, as shown in the same document, and insert the required parameters at the inputs and outputs of the blocks. Once you have studied therm (and the programm examples available in this manual and the First Steps manual also suggested by J_Bell) then we can answer specific questions. Hope this helps, Daniel Chartier |
| 10/27/2007 1:42 PM | |
|
Posts: 23 Rating:
|
DEAR MR... which LEDs should be lighting if communication partner iis not connected to cp341. |
Follow us on