(0)| 10/17/2014 11:30 AM | |
|
Joined: 4/24/2006 Last visit: 1/16/2026 Posts: 9105 Rating:
|
Hello, Perhaps you can use the ET200S Compact. ET 200S COMPACT Released for Delivery Best regards, Wizard |
| 10/20/2014 7:18 AM | |
|
Posts: 4620 Rating:
|
Hello, I agree with our Experts, I too have had a problem like that a while ago and I was advised to go to the ET 200S Compact that is the most similar, the only problem you may encounter (maybe) is in the height of the module (if it has not additional terminals in the lower part of the ET 200L). The ET200L is 100mm high instead of the ET200S is higher (depends on additional terminals that are mounted on the bottom). Have a look the Dimensional Drawing: ET 200L, ET 200L-SC and ET 200L-SC IM-SC Distributed ... - Siemens Distributed I/O System ET 200S - Siemens |
This contribution was helpful to
|
|
Follow us on