(0)| 4/5/2011 10:01 AM | |
|
Joined: 4/29/2010 Last visit: 1/20/2025 Posts: 1557 Rating:
|
Hello, so you have got a PC (flexible RT + running project) and a PC (to look at the runtime). In this case the best solution is to use the Sm@rt Viewer (one the PC without the RT) to look at the PC with the flexible runtime. The Sm@rt Viewer is a single program wich don`t need a flexible installation or a license. At your project you have just to set the option "Sm@rtAccess or Service: Start up Sm@rtServer" at the device settings in the project (the Sm@rtServer need a license). This is all. You can also take a look at the getting started manual there all this is also described: WinCC flexible Getting Started Options best regards |
| 4/5/2011 2:13 PM | |
|
Posts: 37 Rating:
|
Thanks Sandman, Is there a product number for the sm@rt viewer software, could not find it in catalogue.
|
Follow us on