(0)| 11/14/2014 10:00 AM | |
|
Posts: 5225 Rating:
|
Hi there, The LOGO product conference is maybe not where you need to be, unless you wish to install a PLC into your system. I think you are in need of a chip based solution. This forum will be helpful if you need help on testing a network between your product and a Siemens brand PLC (LOGO / S7-1200 / S7-1500 / S7-300 / S7-400 / S7-200) or SCADA. Greetings. w --------------------- [LINK1] [LINK2]... Of course, you do not have to use a chip to implement PROFINET. You can use a software stack and a standard Ethernet controller chip… unless you need motion control, then you need silicon to get the needed update times. You did not need to use a chip for PROFIBUS either. You could use a standard RS485 chip and a software stack. But no one does. They use PROFIBUS chips. The same logic applies to PROFINET. [LINK3] |
Follow us on