(0)| 11/20/2014 12:59 PM | |
|
Joined: 1/3/2006 Last visit: 1/13/2026 Posts: 726 Rating:
|
Hi I have an application where in I need to run the motor in FWD/REV direction. It shall run in FWD direction till FWD is presses and in REV direction till REV button is pressed. Also I need to get the healhty feedback. So have used the following parameters for the said application. //FOR RUNNING IN FWD AND REV DIRECTION P1000= 3 (FIXED SPEED) P1001= 50 (SPEED-1) P1002= -50 (SPEED-2) P1020= R720.0 (DI-1) P1021 = R720.1 (DI-2) P1016 = 2 // FOR GETTING STATUS P730=R52.7 (DO-1) Will this work as desired? Have used theTHISmanual for CU240E-2 DP Regards Manmeet |
Last edited by: manmeet at: 11/20/2014 3:34 PMForget to mention parameter P1016 |
|
Follow us on