11/21/2014 7:38 AM | |
Posts: 2 Rating:
|
Hello, We have a problem with SIEMENS SITRANS F M MAG 5000 (transmitter) + 5100W (sensor). HART communication of MAG 5000 is constantly interrupted with DCS Yokogawa Centum CS 3000 (screenshot in the archive). MAG 5000 is connected to analog module (AAI135H), which supports HART protocol. All connections was done according to Siemens manual, which also was enclosed in archive (plus, foto of connection). All data is transmitted by analog signal and HART, but HART connection constantly interrupted. Because of that operator alarm list is always overflowing. We have 8 the same devises. All of them have the same problem. Link to the archive:https://www.dropbox.com/s/a3xaobg64qwm0to/Siemens.rar?dl=0 Please help me with this problem. |
Follow us on