4/21/2013 1:24 AM | |
Joined: 9/27/2006 Last visit: 9/17/2025 Posts: 12411 Rating:
|
Hello fanana; What exactly do you want to do, and what is the equipment involved? What model relay are we talking about, and do they have a Modbus module installed on the back RS-485 communication port? What model DCS are you planning to use, what interface do they have for Modbus RTU RS-485? Do you have access to DIGSI software to setup and configure the communication ports of the relays? The Siprotec relays are not a product supported by this division of Siemens, rather, they are commercialized by the Energy division. You can find their website, with links to the different models of Siprotec 4 and communication documents here:. http://www.energy.siemens.com/hq/en/automation/power-transmission-distribution/protection/siprotec/ |
This contribution was helpful to
1 thankful Users |
4/22/2013 11:03 AM | |
Joined: 5/13/2012 Last visit: 9/14/2024 Posts: 179 Rating:
|
hello dchartier thanks again what i want exactly is : 1-connect 16 devices have in common IEC 61850 ethernet EN100 module to DCS Modbus TCP/IP RJ45? 2-i know that i should use gateway to convert the output IEC 61850 to modbus so which kind of gateway available for this issues,note that the DCS side dosn't give me any information except i mentioned? 3- i also want to ask additional something if i have RS 485 modbus output from relay which kind of gateway available to connect with DCS and also the communication way how can i collect all devices to connect with gateway.? thank you very much for support me AttachmentD:\SCS\support online\Drawing1.pdf (649 Downloads) |
best regards |
|
4/24/2013 9:17 AM | |
Joined: 5/13/2012 Last visit: 9/14/2024 Posts: 179 Rating:
|
thank you very much mike |
best regards |
|
9/19/2014 9:42 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4759 Rating:
|
New question published by obrowneis split to a separate thread with the subject Where I can buy an RS485 modbus interface card for a SIPROTEC 4?. Best regards Min_Moderator |
12/26/2014 12:09 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4759 Rating:
|
|
Follow us on