(0)| 1/7/2015 1:05 PM | |
|
Joined: 10/28/2014 Last visit: 12/11/2024 Posts: 20 Rating:
|
Hello I have make a simple program , in which i am using a function call . The programs calls a FC block, I am trying to set the output using positive edge of the variable 'test1'. The positive edge of the variable generates a pulse which sets the output of the FC block , which is being use to Set a variable 'test4' in main program block . I tried using the program i have made but couldnt able to update the variable in main program . I want to know what could be wrong . Actually this is the part of one big code which i need to use in my original program I have attached the screenshots of program,The zip file contains 1 )Function call: FC.jpg 2) main program : mainprogram.jpg Thanks Attachmentmainprogram.zip (142 Downloads) |
Follow us on