(0)| 2/19/2015 12:46 PM | |
|
Posts: 2 Rating:
|
Hi, I have a problem related to analog input in my system. In my project I am using siemens S7-1200 PLC (CPU 1214C AC/DC/Rly) With an Analog Input/out module (SM 1234 AI4/AQ2). I am using one of the analog Input for taking weighting value (4-20mA) from a Module; Brand: SEWHA, Model: SI 4100; Normally the module is showing actual weighting result (Say if I put one Kilogram over the load cell its showing 1 kilogram) if I dont connect the analog out (from the weighting) to the PLC's analog input. But if I connect with the PLC then weighting modules Indicator as well as HMI (Connected with the PLC) is showing 5 Kilograms, sometimes 10 kilograms also sometimes correct result 1 Kilogram. I have checked the Weighting module connected with other PLC (LS), its working fine. I have checked with a new analog card but the result is still the same problematic. Hence I will be highly pleased if you suggest me what can do to solve the problem? What can I check? Thanks in advance. Regards Talash Maintenance Engineer (Automation) Dhaka, Bangladesh
------------- |
Last edited by: Min_Moderator at: 2/19/2015 1:14:46 PMNew subject after splitting |
|
Follow us on