(0)| 12/13/2007 9:22 PM | |
|
Posts: 58 Rating:
|
Hello, you need an optional package for configuring Sinaut Connections. http://support.automation.siemens.com/WW/view/en/25585679 Regards, Dreminee |
| 12/16/2007 7:10 PM | |
|
Joined: 1/7/2006 Last visit: 5/11/2025 Posts: 2705 Rating:
|
Hi, You need the connections to generate from TD7 (the program where you made the hardcopys), after that please go to Netpro and load the connections to the different TIMs and CPUs, the hardware is going then dirctly with Netpro. In Netpro you could see which connections are made and the numbers of the connections that are esspecially made for the TIMs. With the compilation of the connections with TD7 also the software for the CPUs is made and must be loaded. If that is all loaded then you could be reached the stations and all the TIMs. Please consider that there are Stations and a Central part, if you use ST7cc later then that could be the Central Station. Please look in the handbooks for the TIM/ST7 and ST7cc: SINAUT ST7 System Manual, Volume 1: System and Hardware SINAUT ST7 System Manual, Volume 2: Software Manual SINAUT ST7cc Control Center |
|
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on