(0)| 12/21/2007 11:48 PM | |
|
Joined: 1/7/2006 Last visit: 5/11/2025 Posts: 2705 Rating:
|
Hi, I have made a small example for you, this is the idea, but it have never seen a CPU from the inside, so it is possible that it not works. However it must be easy to get the data from one side to the other, after loading the Hardware, Netpro and the software the connections must be built up when you look in Netpro Online.... If that is ok then you have to give the functions you want free (enable...) so that the functions could be tested one by one.... Please consider that you must set two merkers for one complete connection (on the BSEND and on the BRECV). Please check the software and place the tested version back so that we have all a working example for the CP342-5 with BSEND/BRECV.......... AttachmentProfibus.zip (598 Downloads) |
|
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on