(0)| 5/26/2015 10:56 AM | |
|
Joined: 6/23/2013 Last visit: 12/16/2025 Posts: 65 Rating:
|
For WinCC OA you can better use the forum at the ETM portal https://portal.etm.at.
PLC tags do not automatically appear in WinCC OA, you need to configure the PLC and add a periphery address to a DPE to get a value from a PLC. In the S7 configuration you can choose what kind of connection to use (PG, OP or other). For the S7-1x00 PLC you need to enable PUT/GET communication, use standard access for the communication block with WinCC OA and use only one connection with the PLC by setting a config entry. |
|
WinCC OA expert |
|
Follow us on