(0)| 3/24/2015 1:12 PM | |
|
Joined: 12/4/2012 Last visit: 12/10/2025 Posts: 7 Rating:
|
Hi all, Anyone can help me? I have almoast same trouble with connection my new notebook Fujitsu Siemens Lifebook E754 to PLC with ethernet connection. Options of my notebook in inserted file. If i connect cable in notebook ethernet and everyone PLC with Eternet connection and i want show accesible device, i use PN/IE and name of notebooks Ethernet card, inmediattely show me error n.0140:017088. The same situation i have if i want connect in STEP7 v5.5 sp2 or TIA v11 SP2 or TIA v13 SP1 upd1 to right type of PLC. I try all, not only in this cause forum. Last udate drivers of ethernet card for windows, reinstall STEP 7, TIA version, setting ethernet to DHCP or concrete IP, all without positive effect. If i want connect with PLC, wich have MPI or Profibus, with other MPI/Profibus adapter, all was OK. But Ethernet is not function. If i use Eth.card directly in Windows, it is good. Ping is function too. Have anyone Idea, what can i do? THX. PS:sorry for bad English. ---------------------------------------------------------------------------------------------------- AttachmentTIA_error.docx (435 Downloads) |
Last edited by: Min_Moderator at: 3/25/2015 10:34:21 AMNew subject after splitting |
|
| 6/19/2015 1:57 PM | |
|
Posts: 4757 Rating:
|
|
Follow us on