(2)| 1/5/2008 12:42 PM | |
|
Joined: 1/7/2006 Last visit: 5/11/2025 Posts: 2705 Rating:
|
Hi Anguraj, Lean and mean is what mentioned here, it is the cheapest CP with a lot of capabilitys, but less then for instance the CP 343-1EX30. You have to check very carefull where you place this CP 343-1CX10, see the information on the customer support: What differences exist in the 300-series Ethernet CPs? Also a very good FAQ is the next one: What are the differences between the Ethernet communication services? So the Lean CP is a Server and a S7-300 is also a Server, the not Lean CP's are also Client !! |
|
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on