(0)| 1/3/2007 9:15 AM | |
|
Joined: 4/24/2006 Last visit: 1/16/2026 Posts: 9105 Rating:
|
Hello Julien Also a Happy New Year Perhaps you can use Report System Error. Here are some links: http://support.automation.siemens.com/WW/view/en/19378840 http://support.automation.siemens.com/WW/view/en/22319131 I hope it will help you. Best regards, Wizard |
| 1/3/2007 9:55 AM | |
|
Posts: 1611 Rating:
|
Hi, do you want to know how to create a System Message, or did you want that when you get a System Message that a other Person get a Message too. greetings, |
| 1/3/2007 12:56 PM | |
|
Posts: 58 Rating:
|
[quote user="Wizard"]Hello Julien Also a Happy New Year Perhaps you can use Report System Error. Here are some links: http://support.automation.siemens.com/WW/view/en/19378840 http://support.automation.siemens.com/WW/view/en/22319131 I hope it will help you. Best regards, Wizard i have the error message system. BUT when the CPU is with a SF, for example if i take two modules of the ET200S, the CPU is in STOP and in SF ( In stop because there isn't the OB86). But in wincc flex, i don't have the message that the CPU is in SF But on the CPU the LED SF is lighted. Thanks Julien |
| 1/3/2007 1:46 PM | |
|
Posts: 1611 Rating:
|
Hi, when i understand you right, you want a message if the PLC are in "STOP". Did you know this FAQ => http://support.automation.siemens.com/WW/view/en/19687561 greetings, |
| 1/3/2007 6:30 PM | |
|
Posts: 58 Rating:
|
[quote user="The Brain"]Hi, when i understand you right, you want a message if the PLC are in "STOP". Did you know this FAQ => http://support.automation.siemens.com/WW/view/en/19687561 greetings, If the CPU is in stop I can displayed it in the alarm archive, because i work in integrated, so i displayed the S7 Message... But if the CPU is in System fault....i can't know it. More i'am looking for free solution. Thanks very much for your help Julien |
| 7/13/2015 3:41 PM | |
|
Posts: 4757 Rating:
|
|
Follow us on