(0)| 7/18/2015 8:06 AM | |
|
Joined: 5/9/2011 Last visit: 9/3/2025 Posts: 71 Rating:
|
Hi HannAri, I don't have access to my TIA portal at the moment however I have attached a small example from Step 7 in FBD that you might find use-full to start your program. It is only a basic example of a sequence start and you will need to modify it to suit your need. I0.5, I0.6 and i0.7 can be the start button for each Mbit or you can replace them with another memory bit and add another SR to set the bit for each output you need to control. I take it you will use a push button N/O for start and N/C for stop? AttachmentSEQUENCE START.pdf (355 Downloads) |
This contribution was helpful to
|
|
Follow us on