(0)| 5/25/2015 11:12 AM | |
|
Joined: 3/31/2015 Last visit: 11/13/2025 Posts: 175 Rating:
|
6SL3255-0VE00-0UA0 is a Parameter Loader 6SL3255-0VA00-2AA0 is BOP interface
BOP Interface - https://cache.industry.siemens.com/dl/files/808/93838808/att_78001/v1/SINAMICS_V20_BOP_interface_module_012014.pdf This module can be used as an interface module for the external BOP, thus realizing the remote control over the inverter by the external BOP, and provides the ability to upload / download parameter sets between the inverter and an MMC / SD card. Parameter loader provides the ability to upload/download peremeters sets between V20 and a SD Card. It has to be removed during normal operation as it's only a commisioning tool. It's needed to clone parameters from one inverter to another. However early this year there was an information published : As the parameter loader provide better usability for parameter cloning, the SD card slot in the BOP interface module will be canceled. So in hardware versions FS 02 and above of BOP Interface there will be no SD card slot anymore. |
This contribution was helpful to
|
|
Follow us on