(0)| 8/15/2015 8:08 PM | |
|
Joined: 1/28/2009 Last visit: 1/5/2026 Posts: 6892 Rating:
|
Dear User, My question is, if one of the power supply PS 407 10A (MLFB 6ES7 407-0KR02-0AA0) in both rack is fail then can I replace with PS 407 10A ((MLFB 6ES7 407-0KA02-0AA0). if possible then, should I need to change PLC hardware configuration for power supply Model..??. I don't think this is possible because to have the functionality explained HERE , you need a PS with redundancy capability.Even HW.Config doesn't accept to use 6ES7 407-0KA02-0AA0 instead of a redundant PS. hdhosseini |
Follow us on