(0)| 9/24/2015 11:26 AM | |
|
Joined: 5/20/2015 Last visit: 1/14/2026 Posts: 221 Rating:
|
hellow freinds i am back with new query as follows: Requirments 1) Event based report generation in custom formate. 2) max power tags are 512 to generate report. 3) Historical report stoarage. considering all the above requirments I WANT TO USE WinCCflexible PC BASED, SO I WANT TO KNOW THE THINGS 1) IS IT NECESSARY TO LOG DATA IN SQL SERVER FOR REPORTING, IF IT IS EVENT BASED. 2) CAN I USE File - CSV (ASCII) TYPE TO LOG DATA IN CSV FORMATE, ON PARTICULAR EVENTS WITH SPECIFIC TAGS, IS THER LIMITATION OF LICENCE. 3) WHICH LICESENCE I NEED TO PURCHASE. IF REPORTING TAGS ARE UNDER 512 PLEASE GUIDE ME ASAP. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 9/24/2015 3:31:19 PMNew subject after splitting Let's do it... |
|
| 10/12/2015 10:46 AM | |
|
Posts: 457 Rating:
|
Hello gabbar, do you got your project solved?
You can store tags or variables in archives (in a SQL, in a csv, in a raw data file) triggered by an Event or cyclic. Please take a look in WinCC flexible Manual, chapter 9. Here you can fnd the Manual: https://support.industry.siemens.com/cs/ww/en/ps/14859/man
I have some examples how to read/write to a file. But maybe, above mentioned Manual will serve you. Best regards Georg |
Follow us on