(0)| 10/28/2015 10:47 AM | |
|
Posts: 2930 Rating:
|
Hi, if you need to change values via the web-server, then you have to allow to change parameters from a FB. If you want to change values in VM-Memory, then use the variable table in the Web-Server, enter the VM-Adress and change the value If you have several LOGO! 8 in a network and you can't access to LOGO!, then check: + in same subnet: If the IP of the LOGO! is correct Attached is a example with different protection and VW0 you can change via Web-Server. Hope this helps Attachmentex_1.zip (374 Downloads) |
| 10/28/2015 11:17 AM | |
|
Posts: 17 Rating:
|
thank you so much for your help can i make a force for input or output ? because i can't find protection check box in input or output |
Follow us on