(0)| 2/8/2008 11:10 AM | |
|
Posts: 5822 Rating:
|
Dear JimR, well this is not really easy. You have actually two choices, as long as you use Windows XP, 2000 or Vista. Because than you can use: - Softnet S7 Lean to Put / Get Data from both PLCs. This is easily made by OPC Server calls... if possible. Here you do not nee to do anything on the PLC. - Softnet S7 Lean with ISO Transport or ISO on TCP with Fetch / Write, also with OPC Server but in this case you have to configure special Connections (one Fetch and one Write)on the S7 CPU. and... last but not least, - Winsock with TCP over Fetch / Write but here you have to program a lot, the Header used in the S7 are explained in the Manual: S7-CPs for Industrial Ethernet Configuring and Commissioning See Appendix E. I hope I could help you with these information's Best regards J_Bell |
Follow us on