11/30/2015 2:54 PM | |
Joined: 10/23/2013 Last visit: 6/12/2022 Posts: 4 Rating:
|
We are upgrading the communication module on the relay 7SJ6322-5EB30-3FD0 from IEC-103 to IEC-61850. Now we have ordered the below material to add to the relay, we need to know if we require any firmware update as well on the relay or just we simply replace the module and change the MLFB number in DIGSI. If yes where can we get this firmware?
61850 MODULE CODE Regards, Altaf Hussain Shaik ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 12/1/2015 1:00:51 PMNew subject after splitting |
|
Follow us on