(1)| 12/19/2015 2:57 PM | |||
|
Joined: 9/27/2006 Last visit: 1/14/2026 Posts: 12481 Rating:
|
Hello Dolpong; For a basic review of the protocols supported by the integrated Profinet port on the CPU and a CP 443-1, have a look at the following FAQ:
Which types of connection/protocols do the S7-300/400 CPUs and the CPs support by default?
https://support.industry.siemens.com/cs/ww/en/view/24352751
You can see that both interfaces support the same basic functionalities (except for ISO Transport protocol, E-Mail and FTP, available only with CPs). However, there are different levels of CP 443-1, and all of the modules do not support all of the functionalities (the CP 443-1 Advanced is the most flexible CP, also the most expensive). And the implementation of the different protocols sometimes require different communication blocks on the CPs and on the integrated Profinet port. For mode details, use the links available in the FAQ. Hope this helps, Daniel Chartier |
||
This contribution was helpful to
|
|||
| 12/20/2015 2:08 AM | |
|
Posts: 45 Rating:
|
Hi, Thank you for your kind and helpful answers. [...] Many thanks again. Attachmentdiagram-2.pdf (708 Downloads) |
Last edited by: Min_Moderator at: 12/21/2015 2:30:14 PMNew question split |
|
| 12/21/2015 2:30 PM | |
|
Posts: 4757 Rating:
|
|
Follow us on