(0)| 12/31/2015 9:08 AM | |
|
Posts: 147 Rating:
|
I have a Vacon driver, uploaded the GSD. It is the manufacturers case to put a manual for Step7 on how to configure the data communication of GSD files in Ste7 5.5 ? I did some Ylink connections to s7-200 PLCs before and configured the communication for 4 bytes out, 4 bytes in I believe . Is it the same case here or would it be different ? knowing that I do not have the Step 7 5.5 software with me yet and I posted this to support a friend of mine, so I am particularly looking for a Siemens manual or a document that can explain the set up of a GSD file and it's communication in details Thank you. AttachmentVac29500.zip (624 Downloads) |
| 12/31/2015 9:31 AM | |
|
Joined: 5/12/2006 Last visit: 1/12/2026 Posts: 22818 Rating:
|
Hello, i think this is the right manual or? The Inverter working with defined PPO telegrams, so the configuration depends of the inverter settings. The principles are described in the manual in the Link.
Christoph |
Follow us on