1/28/2016 8:29 PM | |
Posts: 163 Rating:
|
Hello, Would you like to help connect a Mitsubishi FX-16MR PLC to a Siemens HMI, like a Simatic Panel for example? Regards, |
1/28/2016 9:35 PM | |
Joined: 9/27/2006 Last visit: 9/7/2025 Posts: 12401 Rating:
|
Hello ldir; What type of Siemens panel are you working with, and what software will you use to program them, please. We need some information if you want us to help you. If you are using a panel programmed with WinCC Flexible (TP..., MP...), see the following manual: SIMATIC HMI WinCC flexible 2008 Communication Part 2 https://support.industry.siemens.com/cs/lu/en/view/18797249
Communication partner (Mitsubishi MELSEC)
Introduction
This section describes communication between an HMI device and Mitsubishi Electric controllers.
These controllers communicate by means of the following own protocols:
For this point-to-point connection, the HMI device is connected to the programming interface of the CPU (RS-422).
With this protocol, point-to-point or multipoint connections can be established over Mitsubishi communications modules with RS-232 or RS-422 interfaces.
For information on TIA Portal panels (KTP...), see this table from the Siemens Industry Mall: Controllers from other manufacturers (TIA Portal) https://mall.industry.siemens.com/mall/en/WW/Catalog/Products/10090619 Hope this helps, Daniel Chartier
|
This contribution was helpful to
2 thankful Users |
Follow us on