(1)| 2/10/2016 9:26 AM | |
|
Posts: 12 Rating:
|
hello, If i connect 10 x 8DI DC24V (6ES7131-4BF00-0AA0) on a single power module as mentioned then weather it is compatible or not fo PM module. |
| 2/10/2016 9:42 AM | |
|
Posts: 5521 Rating:
|
hi Rakesh, 10 x 8DI DC24V 6ES7131-4BF00-0AA0 is no problem. DI at all are no problem. Powermodules are for supply the Outputs and the Modules that need power from the power rails in the Terminalmodules. See the manual of ET200s for futher information. Chapter 3.4 SIMATIC Distributed I/O System ET 200Shope this helps, regards, |
Follow us on