12/13/2011 5:02 AM | |
Posts: 1064 Rating:
|
That is right you need a converter , i have heard of some people using a usb to serial converter then a tty to serial interface but i have never tried this check this link it will tell you more /tf/WW/en/Posts/18228 |
12/13/2011 12:21 PM | |
Posts: 376 Rating:
|
Hello, Here some further recommendation. If youuses a PC with serial RS232 interface youcan take the PC converter cable with the order number 6ES5734-1BD20. The interface assignment of the PC converter cable finds you here: http://support.automation.siemens.com/WW/view/en/13063839 Here a further recommendation. Köster-Box (PC-S5-Interface) Interface for programming Siemens S5-PLCs with the PC. The Kösterbox converts the RS232 signals of the PC into TTY signals (20mA) of the automation system. • The box is full duplex, send- and recieve channel, • the box is active for programming S5 90-115U, • for S5-135/155U and CP or acting passively with other cable, • the box has its own power supply with galvanic separation Her the link: http://www.koester-systemtechnik.de/Koester_Box_E.html Best regards Azteke0110 |
This contribution was helpful to
1 thankful Users |
3/14/2016 3:07 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4759 Rating:
|
New question published by lonniealpha is split to a separate thread with the subject 6ES5734-2BF00 cable to connect Field PG4 to OP27. Best regards |
Follow us on