(1)| 3/30/2016 5:14 PM | |
|
Posts: 5 Rating:
|
Hello Friends, I have some questions regarding Sicam PAS UI Configuration. Any help will be very appreciated. 1. On SICAM PAS Configuration, Do you know what is the Interface IP Address for? I'm starting the configuration of a 61850 protocol, adding SEL IEDs. I'm using AcSELerator software to add the devices, configure the IP address and then export CID files, and importing them with Sicam PAS. But I'm not sure what is the IP address on the interface configuration for. 2. I have to add a Power Meter to my configuration, it's a ION7650 from Schneider, connected with SICAM through 61850, but I don't know how to generate the template file of that device to import it into Sicam, I tried with ION Setup, a software to configure this power meters, but I could not do it. 3. Working with Modbus TPC interface, how do I add templates form other manufacturers? I have a lot of devices to add that are Schneider, and I'm having hard time to include them into SICAM with all the mapping that is needed. Finally, I saw in the forums some people offered some manuals and information to help with Sicam configuration. Would you please let me know where can I find this information? Best Regards, Marcos ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 3/31/2016 9:05:55 AMNew subject after splitting |
|
| 3/30/2016 10:02 PM | |
|
Posts: 5 Rating:
|
Thanks Mike, I will work with your recommendations. Regards, Marcos |
Follow us on