(0)| 4/7/2016 11:26 AM | |
|
Posts: 45 Rating:
|
Good morning Expert :) Is it possible to communicate with PROFIBUS DP a CPU 443-1 ref:" 6GK7443-1EX30-0XE0" with an esclave ? If yes How that ? Best regards, |
| 4/7/2016 12:39 PM | |
|
Posts: 433 Rating:
|
And this CP443-1 is an ethernet-CP, not a profibus-CP. Tomcat |
| 4/7/2016 1:25 PM | |
|
Posts: 433 Rating:
|
Hi Wizard, oh, yes. You are right. Tomcat |
| 4/7/2016 1:53 PM | |
|
Joined: 9/7/2007 Last visit: 4/3/2025 Posts: 550 Rating:
|
Hi NACHATE For Using CP443-5 Profibus Dp as a slave is not supported refer o the thread: Use CP 443-5 as slaveAs for CP 6GK7443-1EX30-0XE0 it is a communication processor for connecting a SIMATIC S7-400 to Industrial Ethernet networks, also as PROFINET IO controller or in SIMATIC H systems.The CP supports:
The communications processor can also be used for redundant S7 communication in SIMATIC H systems and for fail-safe applications (PROFIsafe) in connection with an S7-400 F-CPU.
|
|
Best Regards |
|
Follow us on