(1)| 3/11/2008 12:07 PM | |
|
Posts: 8 Rating:
|
Hi Manc: Sorry, I can't help you about that special caracter. But there is another way for sending email from an S7-200. It's Nubitek_Email, a library for MicroWIN that gives you a great flexibility creating the text of the email (up to 1500 caracters). You can download it and test it for free. http://www.nubitek.com/section02/pr02-email.htm Regards, Lorenzo |
| 3/11/2008 12:47 PM | |
|
Joined: 9/29/2005 Last visit: 12/2/2025 Posts: 313 Rating:
|
Hi Manc, yes it should be possible. You can send every ASCII sign you want. But you have do address it as STRING anymore. This means the Sentences "Hello World $&/"" you have to implement in Micro/WIN as following: <<special_chars_handling1.gif>> Have look to this table for special characters in Micro/WIN: Code Interpretation $$ Single dollar sign $’ Single quote character $" Double quote character $L or $l A line feed character $N or $n A new line character $P or $p Form feed, new page $R or $r Carriage return character $T or $t Tabulation, i.e. tab character $1f The two Hex digits 1f after the $ specify ASCII code 1f.ASCII 1f Hex = ASCII 31 Decimal So looking to the last line of the table you can implement each ASCII sign you want. You can also exchange it in the STRING with the move_Byte_command on the correct slot. http://de.wikipedia.org/wiki/ASCII-Tabelle Does this help? Lif |
| 3/14/2008 11:51 AM | |
|
Joined: 9/29/2005 Last visit: 12/2/2025 Posts: 313 Rating:
|
Hi, i had a closer look to the cp243-1it and now its clear. please connect with ftp to your cp. have a look to the directory you see in the attached picture: <<directory_cp342-1-it>> Open the file project1.edb with e.g. notepad <<project1.edb>> Therefore you see all 31 messages. In this case i created two mails 00|TX|This is the Text fo module 1 to Engineer 1 01|TO| ..... Those are the messages you want to change. But notice: The length of a message must not be changed. This means you should implement in the STEP 7-micro/WIN wizard a maximum length. Maybe you fill out the message with dumy signs or blanks e.g. This is the message . <-- notice the dot Ok, how to connect from cpu to cp243-1 internal ftp server. have a look to the attached microwin project. therefore a friend of mine changes the dataname of a file on the ftp server. maybe this will give you some suggestions. <<filename.mwp>> AttachmentDesktop.zip (324 Downloads) |
Follow us on